RealSense Support

D435 depth accuracy without infrared projector

Comments

1 comment

  • MartyG

    1.  The dot pattern projection cast onto surfaces in the scene aids the camera in analyzing surfaces for depth information.  If the projector is off then the depth image will continue to be generated but is likely to have holes in it where no depth data is present. 

     

    Where depth data is present on the image, the depth value may be inaccurate due to the difficulty in reading the surfaces. 

     

    The D455 camera model supports a thermal compensation feature that automatically adjusts the camera's calibration according to the current temperature.

     

    If external lighting is installed near the camera though then it could use that ambient light instead of the dot pattern for depth analysis.  This could be an infrared lamp with invisible light if the outdoor scene must not be illuminated with a conventional visible lamp.

     

    2.  The external temperature of the camera casing can affect the internal operating temperature.  It may be difficult for the internal temperature to drop as far as 0 degrees though so long as the camera is powered and actively streaming.  When the camera is inactive (unpowered), it is rated to withstand exposure to up to -40 degrees C for a short time.

     

     

    Setting the camera's Laser Power setting to its maximum power value of '360' instead of the default of '156' may help to increase internal temperature during operation.

     

    There is not specific data about how extreme cold would affect a RealSense camera's RGB sensor.  In general though, electronics have the potential to become impaired in freezing temperature.  

     

    Just as external casing temperature affects internal temperature, a rise in internal temperature should cause the external casing temperature to rise.

    0
    Comment actions Permalink

Please sign in to leave a comment.