RealSense Support

Maximum Range(Distance) that "Short-range" Preset can give depth with XGA resolution.

Comments

5 comments

  • Yu-Chern Peh

    Hi Aravindjag,

    Based on the L515 datasheet (page 8, Table 3.1 Depth Camera Specification), the maximum distance for L515 with XGA Resolution (1024x768) can reach up to 2.6m at 15% reflectivity and 6.5m at 95% reflectivity. 


    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    -1
    Comment actions Permalink
  • Aravindjag

    Our Question was, what is the maximum distance that "short range" pre-set covers.

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Aravindjag,

    I've validated that the maximum distance for L515 in "Short Range" Preset Control can reach up to 6.5m which is the same as the L515 datasheet (page 8, Table 3.1 Depth Camera Specification).


    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Aravindjag

    Is that 6.5 meters same for "short Range" preset in XGA resolution?

    0
    Comment actions Permalink
  • Yu-Chern Peh

    Hi Aravindjag,

     

    Yes, for the maximum distance for L515 in depth measurement, 6.5 meters can be reached up in "Short Range" Preset Control with XGA Resolution (1024x768).

     

     

    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    1
    Comment actions Permalink

Please sign in to leave a comment.