RealSense Support

Instrinsics and alignement

Comments

2 comments

  • Zulkifli Halim

    Hello Christian Hubert,

     

    Yes, the align-to-color process sets depth stream intrinsics = color stream intrinsics. This can be verified with this code (modified rs-align.cpp):

      int main(int argc, char * argv[]) try
    {
        // Create and initialize GUI related objects
        window app(1280, 720, "RealSense Align Example"); // Simple window handling
        ImGui_ImplGlfw_Init(app, false);      // ImGui library intializition
        rs2::colorizer c;                    // Helper to colorize depth images
        texture depth_image, color_image;    // Helpers for renderig images

        // Create a pipeline to easily configure and start the camera
        rs2::pipeline pipe;
        rs2::config cfg;
        cfg.enable_stream(RS2_STREAM_DEPTH);
        cfg.enable_stream(RS2_STREAM_COLOR);
        pipe.start(cfg);

        // Define two align objects. One will be used to align
        // to depth viewport and the other to color.
        // Creating align object is an expensive operation
        // that should not be performed in the main loop
        rs2::align align_to_depth(RS2_STREAM_DEPTH);
        rs2::align align_to_color(RS2_STREAM_COLOR);

        float      alpha = 0.5f;              // Transparancy coefficient
        direction  dir = direction::to_color;  // Alignment direction

        while (app) // Application still alive?
        {
            // Using the align object, we block the application until a frameset is available
            rs2::frameset frameset = pipe.wait_for_frames();

            if (dir == direction::to_depth)
            {
                // Align all frames to depth viewport
                frameset = align_to_depth.process(frameset);
            }
            else
            {
                // Align all frames to color viewport
                frameset = align_to_color.process(frameset);
            }

            // With the aligned frameset we proceed as usual
            auto depth = frameset.get_depth_frame();
            auto color = frameset.get_color_frame();
            auto colorized_depth = c.colorize(depth);

            auto depth_profile = depth.get_profile();
            auto depth_stream_profile = depth_profile.as<rs2::video_stream_profile>();
            auto depth_intrin = depth_stream_profile.get_intrinsics();
            auto principal_point = std::make_pair(depth_intrin.ppx, depth_intrin.ppy);
            auto focal_length = std::make_pair(depth_intrin.fx, depth_intrin.fy);
            rs2_distortion model = depth_intrin.model;

            std::cout << "Depth Principal Point        : " << principal_point.first << ", " << principal_point.second << std::endl;
            std::cout << "Depth Focal Length            : " << focal_length.first << ", " << focal_length.second << std::endl;
            std::cout << "Depth Distortion Model        : " << model << std::endl;
            std::cout << "Depth Distortion Coefficients : [" << depth_intrin.coeffs[0] << "," << depth_intrin.coeffs[1] << "," <<
                depth_intrin.coeffs[2] << "," << depth_intrin.coeffs[3] << "," << depth_intrin.coeffs[4] << "]" << std::endl;

            auto color_profile = color.get_profile();
            auto color_stream_profile = color_profile.as<rs2::video_stream_profile>();
            auto color_intrin = color_stream_profile.get_intrinsics();
            auto c_principal_point = std::make_pair(color_intrin.ppx, color_intrin.ppy);
            auto c_focal_length = std::make_pair(color_intrin.fx, color_intrin.fy);
            rs2_distortion c_model = color_intrin.model;

            std::cout << "Color Principal Point        : " << c_principal_point.first << ", " << c_principal_point.second << std::endl;
            std::cout << "Color Focal Length            : " << c_focal_length.first << ", " << c_focal_length.second << std::endl;
            std::cout << "Color Distortion Model        : " << c_model << std::endl;
            std::cout << "Color Distortion Coefficients : [" << color_intrin.coeffs[0] << "," << color_intrin.coeffs[1] << "," <<
                color_intrin.coeffs[2] << "," << color_intrin.coeffs[3] << "," << color_intrin.coeffs[4] << "]" << std::endl;

    Send us your code and pictures or video of your observations so that we can troubleshoot further.

     

    Regards,

    Zulkifli Halim

    Intel Customer Support 

    1
    Comment actions Permalink
  • Christian Hubert

    Hello Zulkifli Halim,

     

    Effectively, in mean time I was able to see that the intrinsics are aligned. So this subject is ok and be closed.

     

    My issue is more about ArUco accuracy (and other things), but that may be another topic.

     

    Thanks for your answer above.

     

    Regards,

    Christian Hubert

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.