Intel Realsense Viewer not streaming data in 3D view/ nothing exports (L515)
HI all,
I am having serious trouble connecting my L515 to intel realsense viewer. It shows that my L515 is connected via USB 3.2 however it does not stream any data in 3D viewer(pic1) and exports a completely empty point cloud (pic2).
In 2D view it shows something (pic3). however, there is no export data as I mentioned before.
pic1 (3D view)

pic2 (exported data)

pic3 (2D view screenshot)

-
(assign)Hi Forstyhe,
Could you try the workaround below and see if this can fix the issue.
- Use the latest firmware and RealSense SDK 2.0 version.
-
Connect the camera directly to a USB 3 port on your PC.
If the camera is already connected directly to the PC, try using a powered USB hub. -
Use the USB cable that came with the RealSense camera.
The cable that came with your RealSense Camera is a high-quality USB cable that is capable of handling the power and bandwidth requirements of the camera. Using other cables is not recommended. -
Connect the RealSense camera to a different computer - preferably a computer with an Intel processor.
If your camera works on another computer, then the original computer probably has a USB subsystem that the camera is having problems with. -
Flip the USB C connector that is inserted into the camera and re-insert it the opposite way.
Sometimes the camera will work only if the cable is inserted in a particular orientation. -
Update the USB drivers on the PC.
You probably already have the latest USB drivers due to automatic Windows Updates but this is worth checking.
Regards,
Aznie
Intel RealSense Customer Support
Please sign in to leave a comment.
Comments
3 comments