RealSense Support

RGB Module white image

Comments

28 comments

  • MartyX Grover

    Hi Simeonb  Could you left-click on the small up-arrow in the bottom corner of the Viewer window please to open the Debug Log interface and then activate the RGB stream and let me know what the log says (posting an image here if possible).

     

     

    0
    Comment actions Permalink
  • Simeonb

    Hi MartyG

    0
    Comment actions Permalink
  • MartyX Grover

    Thank you very much.  The white display does not look like a typical Frames Not Received scenario, as those words would be displayed in red lettering at the center of the RGB panel if it were.  It more closely resembles the momentary blank white panel after enabling the stream before the usual RGB video display appears.

    As you have changed the cables and tried the camera on two different computers with the same result, it would suggest that it is not the cables or computers that are the source of the problem.

    Is the RGB stream able to appear if you only enable RGB and no other stream types or does it continue to be plain white?

    0
    Comment actions Permalink
  • Simeonb

    Hi  MartyG it does not make a difference. The stream remains white.

    0
    Comment actions Permalink
  • MartyX Grover

    Thank you.  Could you open the Windows Device Manager interface and check under its Cameras category for whether there are two RealSense drivers there, a Depth driver and an RGB driver.

     

    0
    Comment actions Permalink
  • Simeonb

    Hi MartyG Yes both drivers are there.

    0
    Comment actions Permalink
  • MartyX Grover

    Please right-click on the Intel AVStream Camera 2500 driver and select the Disable device option to disable this camera (you can re-enable it again at any time if you need to by right-clicking on the disabled device and selecting Enable device).  This will demonstrate whether the AVStream camera is interfering with the RealSense camera's ability to stream RGB.

    0
    Comment actions Permalink
  • Simeonb

    Thanks MartyG, but still white image. 

    0
    Comment actions Permalink
  • MartyX Grover

    Has the RGB ever functioned or has it always been white since you purchased the camera?

    0
    Comment actions Permalink
  • Simeonb

    MartyX Grover It worked fine until yesterday!

    0
    Comment actions Permalink
  • MartyX Grover

    When you start the RGB stream, does the information at the top of the panel update or are the values frozen?

     

    0
    Comment actions Permalink
  • Simeonb

    MartyG they update

    0
    Comment actions Permalink
  • MartyX Grover

    Thanks very much.  Are you using the standalone version of the RealSense Viewer downloaded from the Assets file list of the RealSense SDK 'Releases' page (Intel.RealSense.Viewer.exe)?

    If not, could you download it please and launch the .exe file at the location where you downloaded it to (do not use the Viewer shortcut icon on the Windows desktop if you have one) and then try enabling the RGB stream in that Viewer.

    https://github.com/IntelRealSense/librealsense/releases

     

    0
    Comment actions Permalink
  • Simeonb

    I tried them both. I reinstalled the Intel.RealSense.Viewer.exe just now but there are no changes

     

    0
    Comment actions Permalink
  • MartyX Grover

    I appreciate your patience during this diagnostic process. Next, could you try disabling the GLSL options in the Viewer's settings using the instructions in the link below to see whether it makes a positive difference to performance.

    https://github.com/IntelRealSense/librealsense/issues/8110#issuecomment-754705023

    0
    Comment actions Permalink
  • Simeonb

    Thank you for your time  MartyG! There are no changes to the performance.

     

    There is a new line in the Debug Console. (line 3: 16.06.11)

    0
    Comment actions Permalink
  • MartyX Grover

    You are very welcome   :)

    The log message Found 1 unreachable streams enabled me to find a similar past case with a D435i and Windows where this error had occurred and the RealSense user in that case experienced the error on multiple PCs.

    https://support.intelrealsense.com/hc/en-us/community/posts/360048388253/comments/360012184553

    In that case, I suggested performing a gold reset procedure on the camera to reset it to its factory-default settings.

    https://support.intelrealsense.com/hc/en-us/community/posts/360048388253/comments/360011983294

    0
    Comment actions Permalink
  • Simeonb

    MartyX Grover I managed to do the gold reset shown below. Bot there is still a white screen

    0
    Comment actions Permalink
  • Simeonb

    the same message appears again. But allways the second time starting the rgb-stream after connecting the camera to the pc

    0
    Comment actions Permalink
  • MartyX Grover

    Any change if you select a different format for the RGB stream from the drop-down selector before enabling the stream, such as YUYV?

     

    0
    Comment actions Permalink
  • Simeonb

    MartyG using YUYV I get a load of error messanges:

    Same for all the other options.

    0
    Comment actions Permalink
  • MartyX Grover

    It looks as though it is complaining about the OpenVINO face detection mode in the RGB settings of the Viewer.  Given that you had the white-screen problem in the standalone Viewer that does not have OpenVINO, I doubt that disabling it may make a difference but you can try it anyway.

    If the Post-Processing option inside the RGB options section is enabled (a blue icon beside it) then left-click on the blue icon to toggle it to red (off).

     

    0
    Comment actions Permalink
  • Simeonb

    MartyG now they dont send the errors but all change to YUYV.

    exept for RAW16 this message apears on the RGB-frame "The requested format RAW16 is not supported for rendering".

    0
    Comment actions Permalink
  • MartyX Grover

    It is normal for it to produce the message Resolved to: YUYV Color when using the other formats, so that does not indicate a problem.  It is also nornal for RAW16 to not render in the Viewer.

    But you still have no image other than the plain white one no matter which format is used?

    0
    Comment actions Permalink
  • Simeonb

    MartyX Grover Yes still only white

    0
    Comment actions Permalink
  • MartyX Grover

    At this point I will bring this case to the attention of an Intel RealSense Customer Support team member to seek their advice.

    Hi @...  In this case the RGB sensor on a D435i was functioning up until yesterday.  It seems to be able to stream frames but only has an empty white image that is different from No Frames Received as it has no text in the center of the panel.  It has been tested on another PC with the same results, and a wide range of tests performed during the course of this case have not resolved the problem.  Could you provide advice to Simeonb please?  Thanks!

    0
    Comment actions Permalink
  • Simeonb

    MartyX Grover Thank you for your help so far!

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello Simeonb,

    I applaud your and MartyG's perseverance with this issue. Based on the exhaustive troubleshooting, it's safe to conclude your camera is faulty and requires an RMA if it has been purchased within one year. I will send you instructions for RMA in a private email.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.