RealSense Support

Is slam application possible on raspberry pi 4 with t265 camera?

Comments

2 comments

  • Yu-Chern Peh

    Hi Eremteknoloji, 

     

    Since Intel RealSense T265 computes all tracking data on the device, the only hardware requirements are a USB 2 or USB 3 connection that provides 1.5W of power, along with enough memory and compute to boot the T265 and receive the pose data and use it in your application. 

     

    Hence, Raspberry Pi 4 is quite enough to have good slam performance.

     

     

    Regards,
    Yu-Chern​​
    Intel RealSense Customer Support

    0
    Comment actions Permalink
  • Eremteknoloji

    Thanks Yu-Chern. You are great. This is good news. Thank you so much. So glad that I have you.

    0
    Comment actions Permalink

Please sign in to leave a comment.