RealSense Support

Comments

4 comments

  • Jesus Garcia

    Hello Spi,

    Please describe further how to reproduce your issue.

    1. Are you using the rsid-viewer.exe from the binary installation of the RealSenseID SDK or did you build it from source?
    2. Are you using the latest version of the RealSenseID SDK?
    3. Are you trying to enroll or authenticate?
    4. Device or host mode?
    5. Do other RealSenseID SDK tools, such as rsid-cli.exe, work? 
    6. What about the C++ and C sample programs?
    7. Can you send us your log output?

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Spi

    1.Yes i am using rsid-viewer.exe from F450_2.3.0.63_SIGNED.bin

    1. enroll Says enroll failed
    2. I am using  host mode
    3. rsid-cli.exe Says nothing
      1. enroll Says enroll failed
      2. I am using  host mode
      3. rsid-cli.exe Says nothing
      4. Firmware:

        * OPFW - 1.6.1.1007

        * NNLED - 1.3.21.0

        * NNLAS - 10.11.20.0

        * DNET - 4.5.20.0

        * RECOG - 20.12.20.0

        * YOLO - 28.1.20.0

        * AS2DLR - 21.11.20.0

         

        S/N: 10446228094299A27FM10464-100

         

        Pinging device...

        Failed

      5. Firmware:

        * OPFW - 1.6.1.1007

        * NNLED - 1.3.21.0

        * NNLAS - 10.11.20.0

        * DNET - 4.5.20.0

        * RECOG - 20.12.20.0

        * YOLO - 28.1.20.0

        * AS2DLR - 21.11.20.0

         

        S/N: 10446228094299A27FM10464-100

         

        Pinging device...

        Failed

         

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello Spi,

     

    The serial number 10446228094299A27FM10464-100 does not seem to belong to an F455. The serial number is listed on the camera and on the camera box. Can you confirm which serial number is on the camera?

     

    It seems that your F455 is not being properly recognized. To confirm if your PC detects the F455, send us a screenshot of your Device Manager with the following nodes expanded:

     

    Device Manager | Cameras -> should list Intel F450

    Device Manager | Ports (COM & LPT) -> should list USB Serial Device (COM#)

     

    When you run rsid-cli.exe, make sure you use the COM# as: rsid-cli.exe COM# (# shown in Ports (COM & LPT).

     

    Also, upgrade to RealSenseID SDK v.0.16.0 (rsid_sdk_v0.16.0_win64.exe) with firmware version F450_2.4.2.74_SIGNED.bin.

     

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Spi

    after upgrade firmware version wit F450_2.4.2.74_SIGNED.bin. the F450 works properly

    0
    Comment actions Permalink

Please sign in to leave a comment.