RealSense Support

D455 depth image values - what distance is represented?

Comments

1 comment

  • MartyX Grover

    Hi Huawatuam  Pages 17-18 of the data sheet document for the 400 Series cameras provide the following description for how depth is calculated.

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

     

    ******

    The Intel RealSense D400 series depth camera uses stereo vision to calculate depth.  The stereo vision implementation consists of a left imager, right imager, and an optional infrared projector. The infrared projector projects non-visible static IR pattern to improve depth accuracy in scenes with low texture. 

    The left and right imagers capture the scene and sends imager data to the depth imaging (vision) processor, which calculates depth values for each pixel in the image by correlating points on the left image to the right image and via shift between a point on the Left image and the Right image. The depth pixel values are processed to generate a depth frame.  Subsequent depth frames create a depth video stream.

    The depth pixel value is a measurement from the parallel plane of the imagers and not the absolute range, as illustrated.

     

     

    *****

     

    The 'world origin' (0,0,0) of the coordinate system is the center of the left infrared sensor.  The coordinate system is described in the links below.

    https://github.com/IntelRealSense/librealsense/issues/7279#issuecomment-689031488

     

    https://github.com/IntelRealSense/librealsense/issues/7279#issuecomment-690188950

    0
    Comment actions Permalink

Please sign in to leave a comment.