RealSense Support

L515 does not stream infrared when enabling depth stream

Comments

2 comments

  • Jesus Garcia

    Hello Asaf,

    I'm not sure but I think the problem is that you can't get both infrared and depth using the frame callback with pipe.start. If you use pipe.wait_for_frames() you will get both stream types.

    I am checking with engineering on this.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Asaf Anter

    Thanks for the response,

    Before I needed gyro and accelometer(motion frames) I used the pipe.wait_for_frames() method but later when I want to receive motion frames as well, I miss motion frames since the motion frames frequency is much faster than the images frames frequency.

    when I printed the frame number for each stream I saw that the depth, infrared and confidence frames are perfectly synchronized and are incremented by 1 which is great but the gyro and the accel frame number increment by 7 or 10(it make sense because of the frequency difference).

     

    If it's possible to get all these frames with pipe.wait_for_frames(), so I expect that the function return with a rs2::frameset, and it will contains a batch of frames of gyro and accel so I will have no frame drops 

     

    Is there any way to do that?

     

    0
    Comment actions Permalink

Please sign in to leave a comment.