RealSense Support

DWS software not working with L515 camera, possible fingerprint error

Comments

5 comments

  • Jesus Garcia

    Hello Sizenn,

    In order to resolve your issue we need the following information:

    • Camera Serial Number:
    • Email used for Trial Version Registration:
    • Product Key in Trial Version confirmation email:
    • Email used for Production Version Registration:
    • Product Key in Production Version confirmation email:

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Sizenn

    Hello Jesus,

    I bought the license, and the DWS software is working fine now. But I am still having same problem - fingerprints mismatch error when I try to run the sample code in Visual studio. The information you asked for are:
    Camera Serial Number - XXXXXX
    Email address used for both registration and license - XXXXXX
    License#AID=XXXXXXXXXX

    Below are the messages I get in console when I run the sample code:

    [2021-03-30 14:34:51.070] [] [info] [DWSSDK] Attempt to initialize wrapper with handle = -1
    [2021-03-30 14:34:51.072] [] [debug] [DWSSDK] Get num of connected devices...
    [2021-03-30 14:34:51.627] [DWSSDK] [info] [DWSSDK] LOG CREATED
    [2021-03-30 14:34:51.630] [DWSSDK] [info] [DWSSDK] SDK created with mode=0
    [2021-03-30 14:34:51.631] [DWSSDK] [info] [DWSSDK] RGB stream: 1
    [2021-03-30 14:34:51.631] [DWSSDK] [info] [DWSSDK] GYRO stream: 1
    [2021-03-30 14:34:51.632] [DWSSDK] [info] [DWSSDK] OMP threads: 4
    [2021-03-30 14:34:51.633] [DWSSDK] [info] [DWSSDK] SDK_create
    [2021-03-30 14:34:51.633] [DWSSDK] [info] [DWSSDK] looking for files in: C:\Users\sizenn.HLI\Documents_Projects\Intel_real_project\Configuration\static_mode_config.json
    [2021-03-30 14:34:51.636] [DWSSDK] [info] [DWSSDK] Successfully parsed configuration
    [2021-03-30 14:34:51.637] [DWSSDK] [debug] [DWSSDK] check rs2::context...
    [2021-03-30 14:34:51.642] [DWSSDK] [info] [DWSSDK] Preparing background worker...
    [2021-03-30 14:34:51.643] [DWSSDK] [info] [DWSSDK] Initializing player...
    [2021-03-30 14:34:57.637] [DWSSDK] [info] [STREAM] Prepare LibRealsense terminal...
    [2021-03-30 14:34:57.642] [DWSSDK] [info] [STREAM] Prepare LibRealsense terminal... DONE

    Fingerprint length mismatch, status = 3
    [2021-03-30 14:34:57.647] [DWSSDK] [error] [DWSSDK] Fingerprint length mismatch
    [2021-03-30 14:34:57.652] [DWSSDK] [info] [DWSSDK] ~DWSSDK
    [2021-03-30 14:34:57.666] [DWSSDK] [info] [DWSSDK] dws_stop called
    [2021-03-30 14:34:57.668] [DWSSDK] [info] [DWSSDK] pause called. soft stop = FALSE
    [2021-03-30 14:34:57.669] [DWSSDK] [info] [DWSSDK] stop: Locking mutex_process...
    [2021-03-30 14:34:57.669] [DWSSDK] [info] [DWSSDK] Waiting on worker thread...
    [2021-03-30 14:34:57.889] [DWSSDK] [info] [DWSSDK] Waiting on worker thread... DONE
    [2021-03-30 14:34:58.010] [DWSSDK] [info] [DWSSDK] stop: Locking mutex_process... UNLOCKED
    [2021-03-30 14:34:58.097] [DWSSDK] [info] [STREAM] ======================
    [2021-03-30 14:34:58.148] [DWSSDK] [info] [STREAM] Attempt to tun script: C:\Users\sizenn.HLI\Documents_Projects\Intel_real_project\Configuration\logState.txt
    [2021-03-30 14:34:58.270] [DWSSDK] [info] [STREAM] > irb e2 09 1 // laser modulation limit
    [2021-03-30 14:34:58.421] [DWSSDK] [info] [STREAM] Offset: 0x0 => 2E
    [2021-03-30 14:34:58.421] [DWSSDK] [info] [STREAM] > irb e2 0a 1 // laser modulation limit
    [2021-03-30 14:34:58.525] [DWSSDK] [info] [STREAM] Offset: 0x0 => 2E
    [2021-03-30 14:34:58.533] [DWSSDK] [info] [STREAM] > mrd a00e1890 a00e1894 // invalidation configuration
    [2021-03-30 14:34:58.675] [DWSSDK] [info] [STREAM] Offset: 0x0 => 00000000
    [2021-03-30 14:34:58.676] [DWSSDK] [info] [STREAM] > mrd a00e1600 a00e1604 // edges configuration
    [2021-03-30 14:34:58.765] [DWSSDK] [info] [STREAM] Offset: 0x0 => 00000100
    [2021-03-30 14:34:58.803] [DWSSDK] [info] [STREAM] > mrd a00e1894 a00e1898 // Confidence configuration
    [2021-03-30 14:34:58.961] [DWSSDK] [info] [STREAM] Offset: 0x0 => 00000003
    [2021-03-30 14:34:59.080] [DWSSDK] [info] [STREAM] > mrd a00e0b0c a00e0b10 // Sharpness configuration
    [2021-03-30 14:34:59.332] [DWSSDK] [info] [STREAM] Offset: 0x0 => 0000000C
    [2021-03-30 14:34:59.333] [DWSSDK] [info] [STREAM] > mrd a0020ca8 a0020cac // Rast configuration
    [2021-03-30 14:34:59.575] [DWSSDK] [info] [STREAM] Offset: 0x0 => 00000000
    [2021-03-30 14:34:59.589] [DWSSDK] [info] [STREAM] > apd_flyback_values_get // Get flyback values
    [2021-03-30 14:34:59.805] [DWSSDK] [info] [STREAM] state: 1
    isDataValid: 0
    reserved16: 0000
    vSenseReq: 0000
    pwmValue: 0000
    tSenseRead: 0000
    vSenseRead: 0000
    tSenseC: 0
    vSeneseReadV: 0
    reqV: 0

    [2021-03-30 14:34:59.806] [DWSSDK] [info] [STREAM] > RdCalibInfo 12
    [2021-03-30 14:34:59.942] [DWSSDK] [error] [STREAM] Command not found!
    [2021-03-30 14:35:00.029] [DWSSDK] [info] [STREAM] ======================

    C:\Users\sizenn.HLI\Documents_Projects\Intel_real_project\x64\Debug\Intel_real_project.exe (process 23860) exited with code -1.
    To automatically close the console when debugging stops, enable Tools->Options->Debugging->Automatically close the console when debugging stops.
    Press any key to close this window . . .





    0
    Comment actions Permalink
  • Jesus Garcia

    Hello Sizenn,

    Confirming my understanding...

    Your copy of the DWS Viewer Application is working correctly.

    Your sample code is not working due to the fingerprint error.

    Ensure you are using the same license for both programs. Copy the "License" file from the DWS Viewer folder into the folder where your sample executable is: C:\Users\sizenn.HLI\Documents_Projects\Intel_real_project\x64\Debug\

    Let us know the result.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Sizenn

    Hello Jesus,

    Yes you are correct, my copy of DWS Viewer Application is working correctly but  the sample code is not working due to the fingerprint error. And yes I am using the same license file for both programs, and the License file saved into the folder where my executable file is. 

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello Sizenn,

    We are referring your issue to engineering. Please stay tuned for updates.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.