View my account

I’m Lost. Do I need coding skills In Order To Use my depth camera?

Comments

5 comments

  • MartyX Grover

    Hi Qcreative13  Welcome to the RealSense community!  If you are new to RealSense technology then a good place to begin exploring is the official RealSense YouTube channel, which provides a wide range of videos for all skill levels from beginner to advanced.

    https://www.youtube.com/c/IntelRealSense/videos

    You can certainly achieve a lot with your RealSense camera without needing to do any programming, thanks to the powerful RealSense Viewer tool.  This will enable you to generate 3D scans and export them in a file for use in other software such as 3D modelling packages.

    As a next step, I recommend installing the RealSense SDK software (within which the RealSense Viewer tool is bundled).  Are you using Windows 10 or Linux operating system on your computer, please?

    1
    Comment actions Permalink
  • Qcreative13

    Oh ok thank you for the information. I am running Windows 10

    0
    Comment actions Permalink
  • MartyX Grover

    If you are using Windows 10 then there is an easy method for installing the RealSense SDK software.  This will also place launch icons on your Windows desktop for the RealSense Viewer and a tool called the Depth Quality Tool for evaluating the quality of the depth imge that you are receving from the camera.

    STEP 1

    Visit the Releases page at the link below and scroll down until you find an Assets list.  If it is shown as just the word Assets with a triangle beside it, left-click on the arrow to expand the list open.

    https://github.com/IntelRealSense/librealsense/releases

    In that list, left-click on the file link that starts with the name Intel.RealSense.SDK-Win10 to begin downloading it at the bottom of your browser window. 

     

     

    STEP 2

    When the download is complete, left-click on the download at the bottom of your screen to launch the RealSense SDK installer program.

    You do not need to change anything in the installer's settings.  Just keep clicking Next until the short installation process is complete.

     

     

     

    1
    Comment actions Permalink
  • Qcreative13

    Wow thanks for all the help! Everything is installed that was incredibly helpful thank you

     

    0
    Comment actions Permalink
  • MartyG

    You are very welcome.  :)   When you are ready, please feel free to ask about the questions raised in your opening message, such as creating 3D scans and tracking body motion.  Good luck!

    0
    Comment actions Permalink

Please sign in to leave a comment.