Not able to start the L515
Hi,
I would like to connect a L515 to a Windows 10 computer. When I connect the camera to the computer it is recognized by windows but I have the error message Driver unavailable. What I have done
- Trying multiple computer : same result
- Changing USB 3 port : same
- Did all Windows updates.
- I have tried to use rs-fw-update.exe -l but it said that no connected device
- I have also tried other camera like a D455 without any issue. It works great.
What is the issue with the L515
Thank you
-
Hello Grsabourin,
There are a couple of things you can try to get the L515 properly recognized by your PC.
-
Flip the USB C connector that is inserted into the camera and re-insert it the opposite way.
Sometimes the camera will work only if the cable is inserted in a particular orientation. - Update the USB drivers on the PC.
You probably already have the latest USB drivers due to automatic Windows Updates but this is worth checking.
Please provide the information below to help us diagnose the issue.
PC Information
- PC manufacturer
- PC model number
- Camera serial number - the serial number can be found on the box, on the camera, or in RealSense Viewer.
Answers to the following questions will help us diagnose possible causes of the issue and will not affect your warranty.
- Did this happen on the first connection straight out of the box?
- How is the camera mounted?
- Are you using the tripod and cable that came with the package?
- Was the camera dropped?
- Was the camera banged against an object?
- Can you describe any physical impacts on the camera?
- Are you connecting the camera to a USB hub? If so, which one?
Sincerely,
Jesus G.
Intel Customer Support -
Flip the USB C connector that is inserted into the camera and re-insert it the opposite way.
-
Few answers
Main computer I have tested on is
Dell Precision M4800
numbers on camera : k69571-100, F0246014 999NGF
On the box :
Product code : 82638L515G1PQR
SN : F0246014
- Did this happen on the first connection straight out of the box?
- Yes
- How is the camera mounted?
- Hold in hands for now
- Are you using the tripod and cable that came with the package?
- No
- Was the camera dropped?
- No
- Was the camera banged against an object?
- No
- Can you describe any physical impacts on the camera?
- Never happen
- Are you connecting the camera to a USB hub? If so, which one?
- Direct connection to computer
-
Thank you for the information, Grsabourin.
Based on your description, the camera is faulty and should be returned to the place of purchase.
- If you purchased the unit from the Intel RealSense Store, please sign in to your account on http://www.intelrealsense.com and go to My Account -> My Orders -> Return or Replace Items or open a ticket here.
- If you did not purchase the unit from the Intel Store, contact your distributor for a return.
We apologize for the inconvenience this has caused.
Sincerely,
Jesus G.
Intel Customer Support
Please sign in to leave a comment.
Comments
3 comments