RealSense Support

L515 inconsistent frame counts with external trigger

Comments

3 comments

  • Jesus Garcia

    Hello T Loomans,

    When the sync signal is low and the device is in slave mode, the only features that are turned off are the laser and the pipe (USB transfer) to the host computer. The depth can continue to stream in this case but it's pretty much throw away data since the laser is turned off.

    When the sync signal is high, there is a 60ms setup time to turn on the laser and turn on the pipe before good depth from that camera is realized.

    Pulse width = 60ms(setup) + #of frames33ms
    For example: for capturing 3 consecutive frames Ton needs to be high for 160ms

    So setup time is about 2 frames (60ms ~= 2*33ms) before a good frame is available.

    It will depend on where in the cycle the sync signal is high. You may go high with the sync signal when a frame is already in the middle of its presentation.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • T Loomans

    Dear Jesus,

     

    Thank you for the fast response. However, the conclusion is rather disappointing. Now that you've explained how it works, the answer to my previous support question is actually incorrect (I asked if the setup time was exactly 60.000ms and if the capture starts immediately after this setup time). Also the information in the whitepaper is incorrect (or at least incomplete). Could this be updated so the others might benefit from this information? It would have spared me a lot of time setting up experiments to confirm this behavior if this information was in the whitepaper.

     

    Now that we now that the external trigger can fall in the middle of a cycle resulting in unpredictable delays till the frame is transferred, what is the use of this external trigger port? Because I don't think it can be used to synchronize cameras since they won't be running in exactly the same cycle.

     

    In my setup I want to synchronize the frames of the camera with a conveyor belt with rotary encoder. Not knowing how long after the trigger the frame is taken makes this very difficult. One solution might be if the camera could send the exact timestamp of the last time that the trigger had a rising edge with the frame metadata. Then I could check the difference between the trigger time and the frame time so I know how long its setup time took and compensate for that in the movement of the conveyor. Would it be possible to implement this in the firmware?

    With kind regards.

     

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello T Loomans,

    We are working with engineering on this. Stay tuned for an update.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink

Please sign in to leave a comment.