RealSense Support

Multi People Tracking

Comments

3 comments

  • MartyG

    Hi David  A RealSense team member provides advice in the link below about efficiently obtaining the depth of a specific RGB pixel.

    https://github.com/IntelRealSense/librealsense/issues/6239#issuecomment-614261704

    Python code for the rs2_project_color_pixel_to_depth_pixel instruction referenced in the advice can be found in the link below

    https://github.com/IntelRealSense/librealsense/issues/5603

     

    Edit: on reflection, given that you are aiming to retrieve the world coordinates, using depth-to-color alignment and deprojection may be more suited to your application.

    https://github.com/IntelRealSense/librealsense/issues/3688

    0
    Comment actions Permalink
  • David

    Hi MartyG

    First of all, thank you for sending those reference links ...

    I could use DeProject, but could not go much further...

    Here's what i got:

    camera_coords = rs.rs2_deproject_pixel_to_point(depth_intrin, CenterPt,  distNum)

    depth_Intrin  is the camera intrinsics data got from: depth_intrin = depth_frame.profile.as_video_stream_profile().intrinsics

    Here one note: All the data got from the method above seems to be ok except for the distortion model, which for the case of D415 should be Inverse  Brown-Conrady, but in my case it is returning None.

    CenterPtare the pixel coordinates got from center of the ROI rectangle (got by YOLO  function ... tracking people).

    distNum: as i could understand from the API documentation this should be the depth value (float), got from the depth stream...

    I tried to use  get_distance(x,y) to get the depth value using:  distNum2 = depth_frame.get_distance(xC,yC)

    But it’s returning zero… So, the value i fed into deproject function was the one i got from the depth array … (as below):

    depthData_array = np.asanyarray(depth_frame.get_data())

    distTrackedPeople = depthData_array[yC, xC]

    yC and xC being the pixel coordinates of the tracked people (simple geometric center of bounding rectangle).

    In the plan drawing (below)  you can see the values got from deproject_pixel _to_point() … referenced as POS 1 and POS 2, which are positions registered from the tracked people in 2 arbitrary locations.

    My questions:

    - I assume that rs2_deproject_pixel_to_point() returns  the X,Y,Z coordinates in relation to the Camera Coordinates system. Is that assumption correct ?

    - Does depth_frame.get_distance(xC,yC) ... returns the Euclidean distance from one point in the image and the center of depth  sensor ?

    - Considering the values returned as Camera Coord. System, i made some projections perpendicular do the camera axis, and some of the values returned by deproject does not make much sense. Mainly X of Position 1.

    Once i could understand well  those camera coordinates, getting world coordinates is an easy step (only requires to know the camera translation, rotation of the camera in relation to the origin of the axis in actual camera. And applying those extrinsics to the coordinate results captured by the camera.

     

    0
    Comment actions Permalink
  • MartyX Grover

    The Python case linked to below that describes how to deproject a color pixel with rs2_deproject_pixel_to_point may be helpful to you.

    https://github.com/IntelRealSense/librealsense/issues/2458

    In regard to your questions:

    1.  The camera coordinate system's world origin (0,0,0) is the center of the left infrared imager.  More information about the coordinate system can be found in this link:

    https://github.com/IntelRealSense/librealsense/issues/7279#issuecomment-689031488

    Within that discussion, a RealSense team member provides further detailed explanation of the coordinate system:

    https://github.com/IntelRealSense/librealsense/issues/7279#issuecomment-690188950

    2.  The documentation for depth_frame.get_distance states that it returns "the depth in meters at the given pixel".

    https://intelrealsense.github.io/librealsense/doxygen/classrs2_1_1depth__frame.html#a5090d69d04ade6dd67175cae9b6bee9c

    0
    Comment actions Permalink

Please sign in to leave a comment.