RealSense Support

Intel RealSense LIDAR L515 not being detected by windows after firmware update via Intel.RealSense.Viewer.exe (2.41.0.2657)

Comments

3 comments

  • Zulkifli Halim

    Hello Takeemlowe,

     

    Thank you for contacting us.

     

    The camera might be in a recovery state.

     

    In such a case, you can use the recovery flag and run rs-fw-update -r -f <path_to_Firmware_Image_file>\Signed_Image_UVC_<Firmware_Version>.bin.

     

    The latest firmware for L515, it is available here.

     

    Note that, rs-fw-update.exe is located in the same directory as rs-enumerate-devices.exe. 

     

    Please refer rs-fw-update Tool to get more information on this operation.

     

    Regards,

    Zulkifli 

     

    0
    Comment actions Permalink
  • Takeemlowe

    Thank you. This solved the problem. 

    However, this only works on the system that the camera was previously installed on when it failed to be detected on windows after the update.

    Thank you. 

    0
    Comment actions Permalink
  • Zulkifli Halim

    Hello Takeemlowe,

     

    Thank you for confirming your problem is resolved. I am glad to hear that from you.

     

    I will close this case now. Please open a new case if you have any further issues and we'll be happy to help you.

     

    Regards,

    Zulkifli

    Intel Customer support 

    0
    Comment actions Permalink

Please sign in to leave a comment.