RealSense Support

D455 cannot use OEM Calibration Tool (ver. 1.5.5.0).

Comments

2 comments

  • Brice Miramont

    Hi, did you buy the oem calibration toolkit to oem calibrate the d455 ? I have the same need.

     

    thank you,

     

    Brice

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Brice Miramont  The main advantages of the OEM version of the Dynamic Calibration tool are to (1) calibrate both intrinsics and extrinsics, (2) calibrate remotely via a Linux server, and (3) be able to calibrate multiple cameras.  

    The free non-OEM version of the Dynamic Calibration tool only calibrates extrinsics.  This is sufficient though for the needs of 99% of RealSense users, as it is extrinsics that will have the most effect on the image.  This tool might therefore be sufficient for you.

    https://www.intel.com/content/www/us/en/download/645988/intel-realsense-d400-series-dynamic-calibration-tool.html

     

    The more recent On-Chip Calibration system can calibrate both the intrinsics and extrinsics of depth, though only one or the other at a time rather than both simultaneously.  On-Chip calibration is accessible through the More option of the RealSense Viewer tool's side-panel or with program scripting.  Intel have publised a white-paper guide about On-Chip calibration.

    https://dev.intelrealsense.com/docs/self-calibration-for-depth-cameras

    On-Chip calibration is built into the camera firmware driver and so does not require a separate software package like the Dynamic Calibration tool does.

    0
    Comment actions Permalink

Please sign in to leave a comment.