View my account

Comments

4 comments

  • MartyX Grover

    Hi Chicagobob123  The D455 has 2x the depth accuracy over distance of the D435 model.  So the D455 has the same accuracy at 6 meters as the D435 has at 3 meters. 

    The D435 and D455 have different minimum depth sensing distances (MinZ).  The D435 has a minimum depth distance of 0.1 meters, whilst the minimum depth distance of the D455 is 0.4 meters.

    0
    Comment actions Permalink
  • Jesus Garcia

    Hello Chicagobob123,

    What enables the D455 to detect depth further than the D435 is the longer baseline of the D455, which is the distance between the two depth senors.

    D435 Baseline: 50mm

    D455 Baseline: 95mm

    The longer the baseline, the further the camera can detect depth.

    Sincerely,
    Jesus G.
    Intel Customer Support

    0
    Comment actions Permalink
  • Chicagobob123

    It would be interesting to make the baseline adjustable so it can be extended based on need.  

    Currently its 3.74016 inches, following your logic if you made it about 1 foot baseline it could see 4 times

    farther or about 120 feet. That would be useful for many. 

    The feature set and feedback are great. The 455 has the T265 data and pose information built into it right?

    0
    Comment actions Permalink
  • Jesus Garcia

    Yes, a longer baseline would allow depth sensing much further but trade-offs have to be made based on target usages.

    The T265 is the only camera that provides pose information.

    The D435i, D455, and L515 have built-in IMUs which provide gyro (angular velocity) and accel (angular acceleration) data only, no pose.

    0
    Comment actions Permalink

Please sign in to leave a comment.