RealSense Support

Realsense Install Ubuntu 20.04 Raspberry PI 4

Comments

2 comments

  • MartyG

    Hi Russ  For installing Ubuntu 20.04 on Pi 4, I recommend building librealsense from source code with CMake using the RSUSB installation method and installing the Python wrapper at the same time as building librealsense.

    An RSUSB build uses the CMake build flag -DFORCE_RSUSB_BACKEND=ON to install librealsense over an internet connection without dependence on Linux versions or kernel versions, and with no need for patching.

    The link below leads to instructions for building librealsense and Python together on Jetson and Ubuntu with the RSUSB method.  As Raspberry Pi has an ARM processor like Jetson boards do, it should be a reliable guide for Pi also.

    https://github.com/IntelRealSense/librealsense/issues/7905#issuecomment-737544294 

    Leave out the CMake flag  -DBUILD_WITH_CUDA:bool=true though for Pi, as that command is not supported on Pi boards because they do not have an Nvidia graphics GPU.

    0
    Comment actions Permalink
  • Russ

    I'll give it a shot.

    Thanks MartyG

     

    0
    Comment actions Permalink

Please sign in to leave a comment.