RealSense Support

Can't install Realsense UWP-Driver

Comments

2 comments

  • MartyX Grover

    Hi Mario Heinz  The latest UWP driver version at the time of writing this (6.11.160.21) has caused errors for a small number of RealSense users, specifically with the C# wrapper, Unity wrapper and the Dynamic Calibrator tool.  I would therefore recommend using the earlier 6.1.160.14 version of the driver if you need to use UWP.

    https://downloadcenter.intel.com/download/28723/Intel-RealSense-D400-Series-Universal-Windows-Platform-UWP-Driver-for-Windows-10 

    The UWP driver is not a requirement to use RealSense with Windows though.   It provides RealSense with compatibility with products that support the Universal Windows Platform (UWP) interface, such as the Microsoft Hololens headset.   It can be safely removed if you do not need it.

    0
    Comment actions Permalink
  • Mario Heinz

    Hi MartyG, thank you for your fast response. We are indeed developing a software tool using the C# wrapper. I just realized, that disabling the Windows 10 driver signature enforcement allows me to install the driver correctly. 

    0
    Comment actions Permalink

Please sign in to leave a comment.