D457 registers
Hello, I'm trying to communicate with the D457 using I2C via MIPI CSI2 deserialized with a max9296. I'm referencing Intel's realsense mipi platform (https://github.com/IntelRealSense/realsense_mipi_platform_driver) where the authors were able to read the registers of the D457 using addresses such as 0x5020. Is there a datasheet that contains a register map for the D457?
-
Hi Aslan Chui The bottom of the MIPI platform driver page states that the register values relate to MAX9296 (the deserializer component that is external to the D457 camera)

I conducted an extensive search for a register list for MAX9295 and MAX9296 but the information was not available publicly, unfortunately.
If you have not yet seen the datasheet document for D457, it is available at the link below but does not contain MAX9296 register information.
https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet
-
Found MAX9296 datasheet,
https://datasheet.lcsc.com/lcsc/2208101430_Analog-Devices-MAX9296AGTM-V-T_C2913271.pdf
No such luck for MAX9295 though.
Please sign in to leave a comment.
Comments
2 comments