RealSense Support

RealSense D457 USBC mode camera not detected (Ubuntu 22.04).

Comments

3 comments

  • MartyG

    Hi Stakoverflowed  If you look on the casing of the D457 there is a small removable cap.  Under this cap, which can be removed by inserting a pin into a small hole on the cap, are the hardware sync pins, and also additionally on the D457 a mode switch that controls whether the camera is operating in MIPI or USB mode.  The switch is in the MIPI position by default, preventing the camera from being detected on a USB connection.

     

    To use the camera in USB mode, the mode switch should be moved left to the USB position that is labelled under the cap.  A way to do this is to insert a pin at the position labelled MIPI and gently move the pin sidewards until you feel a physical movement. 

    Once the switch is in USB position, the camera will be detected as D455 and have the same performance and feature-set of a D455, with the added IP65 dust and water protection.

     

    1
    Comment actions Permalink
  • Stakoverflowed

    Thank you, this helped me and the camera works now!

    1
    Comment actions Permalink
  • MartyG

    You are very welcome!

    0
    Comment actions Permalink

Please sign in to leave a comment.