View my account

D435F operation in darkness

Comments

3 comments

  • MartyG

    Hi Roman Leuzinger  The best technical discussions about use of an external IR illuminator with RealSense cameras are at the links below.

    https://github.com/IntelRealSense/librealsense/issues/1070

    https://github.com/IntelRealSense/librealsense/issues/2000

     

    Intel also have a highly detailed white-paper guide about use of external projectors with RealSense 400 Series cameras.

    https://dev.intelrealsense.com/docs/projectors

    0
    Comment actions Permalink
  • Roman Leuzinger

    Thank you for that links. I have read the white-paper already before but have not find a final answer to my uncertainity.

    I understand that the depth noise increases and the resultion decreases when using the IR projector only, especially if it is a IR projector with low dot number.

    However, I do not have too hard requirements:

    Minimimal object size which I want to be able to detect: 100x100mm in 2m distance. And the depth accuracy can be +-20%. I think that would already cover my use case.

    I understand that with IR projector only it will unlikely to detect a wire fence (with 3mm wires) in darkness

    Under this conditions do you see it reasonable to operate the D435F without external IR illumination?

    0
    Comment actions Permalink
  • MartyG

    My understanding is that the built-in IR projector's output is suitable for up to 2 m distance from the camera in darkness conditions, and that an IR illuminator would be recommendable if you needed to provide the camera with sufficient IR light to capture objects / surfaces more than 2 m away.

    0
    Comment actions Permalink

Please sign in to leave a comment.