RealSense Support

D 435 buffer memory

Comments

2 comments

  • MartyG

    Hi Mohammadmahmoodi8020   RealSense 400 Series cameras store the firmware driver and calibration information in small flash memory spaces on the camera hardware but do not store camera stream data.  

     

    Stream frames can be stored in the computer's memory using a RealSense SDK instruction called Keep() though this requires a computer with a large memory capacity as the available memory is consumed over time as it is filled up with stored frames.  A PC with an average sized memory such as 8 GB could likely retain a maximum of 30 seconds worth of frames unless older frames are released to free up memory.  A PC with a larger memory capacity could store a longer duration's worth of frames.

    0
    Comment actions Permalink
  • Mohammadmahmoodi8020

    I appreciate it. 

    0
    Comment actions Permalink

Please sign in to leave a comment.