Question on D405
-
Hi Redyoung A key difference between D405 and D435 / D455 is that the D405 model does not have a separate RGB sensor, as RGB is instead provided by the depth sensor. So a program may fail on D405 if the code has a check to see whether an RGB sensor can be detected. That is an error that would not usually be triggered by the cfg / configuration part of the script though.
Could you post the 'configuration' lines from your script in a comment, please? Thanks!
-
Dim pipeline As New Pipeline
Dim cif As New Configcif.Enablestream(Intel.Realsense.Stream.Depth, 640, 480, format.Z16, 60)
cif.Enablestream(Intel.Realsense.Stream.Infrared, 640, 480, format.Y8, 60)
cif.Enablestream(Intel.Realsense.Stream.Color, 640, 480, format.Bgr8, 60)
cif.EnableDivce (serialNumber)
pipeline.Start(cif)Above are lines that make D435/D455 running but does not work with D405. I tried without colorstreaming and the result was the same.
Thanks in advance for your help here! -
Does the code below work?
var pipeline = new Pipeline();
var cfg = new Config();
cif.EnableStream(Stream.Depth, 640, 480, Format.Z16, 60);
cif.EnableStream(Stream.Infrared, 640, 480, Format.Y8, 60);
cif.EnableStream(Stream.Color, 640, 480, Format.RGB8, 60);
cif.EnableDevice(serialNumber);
pipeline.Start(cif); -
Assuming then that the problem is not with the cif configuration lines, I recall a D405 case from October 2022 where a RealSense user of C# had a crash error with D405 that did not occur with D435.
https://github.com/IntelRealSense/librealsense/issues/10967#issuecomment-1269995345
Are you using the x86 or x64 version of the RealSense DLLs with the C# wrapper? In RealSense SDK 2.50.0 there was a D405-specific crash problem when using D405 with the x86 DLLs (x64 worked fine) that was fixed in SDK 2.51.1.
-
This error can occur if the target platform has been set to 'Any CPU' instead of x86 or x64.
Please sign in to leave a comment.


Comments
10 comments