RealSense Support

Comments

2 comments

  • MartyG

    Hi Matheus Soares  Here is the information that you requested about the RealSense D457.

     

    1.  The Fakra cable in the D457 box has a length of 1000 mm +/- 10

     

    2.  According to RG174 coax cable spec, the minimum radius is 9.9 mm.

     

     

    3.  Users can obtain a longer cable from the market. It is recommended to use “LEONI Dacar 302” for a 10 ~15 m long cable.  RG174 cable has been tried on D457. The maximum length is 11 m, but Dacar 302 can reach 15 m.

    1
    Comment actions Permalink
  • Matheus Soares

    Thanks for your fast reply! That was all the info I needed about the cable.

    0
    Comment actions Permalink

Please sign in to leave a comment.