RealSense Support

Adding Network Modules to Realsense Yocto Layer Build

Comments

3 comments

  • MartyG

    Hi Matthew Derzay  Have you made an ssh connection to the computer that you installed Yocto / librealsense2 on to test whether rs-server can be started (in case it was actually built).  For example from the ethernet guide:

     

    ssh realsense@10.0.0.99
    sudo systemctl restart rs-server.service

    0
    Comment actions Permalink
  • Matthew Derzay

    Hi Marty, yes I can connect to the computer with ssh. I don't have systemd included so I can't use the systemctl command at the moment. But for example when I try to run rs-server, it says command not found. Other commands like rs-enumerate-devices do work so I know at least the basics of the layer are included in the build.

    0
    Comment actions Permalink
  • MartyG

    It looks as though the Yocto layer for librealsense uses the master branch of the librealsense GitHub, meaning that the latest version of librealsense should be installed.  So your librealsense build should have the capability to use networking if the CMake build flag -DBUILD_NETWORK_DEVICE=ON is used.

     

    The rs-server networking support was added in librealsense SDK version 2.34.0 and present in all subsequent versions.  Can you confirm which librealsense version is installed, please?

    0
    Comment actions Permalink

Please sign in to leave a comment.